Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Mouser Now Shipping All Three Popular UDOO Neo Boards

December 8, 2015 - Mouser Electronics, Inc. is now shipping the highly anticipated Neo single-board computers from UDOO.

The UDOO Neo boards, now available from Mouser Electronics, are open-source, low-cost computers available in three models: Basic, Extended, and Full. Each Neo board is equipped with a Freescale i.MX 6 SoloX applications processor with a 1GHz ARM® Cortex®-A9 core for Android and Linux, and an embedded ARM Cortex-M4 microcontroller, which makes the boards compatible with the Arduino environment.

The Neo boards offer 54 general-purpose inputs and outputs (GPIO), including two sets of I/O headers: One that meets the Arduino Uno form factor for use with Arduino shields, and an additional set that provides extended I/O functionality. Through the headers, engineers can access USB, I2C, SPI, UART, and CAN bus interfaces and eight PWM signals. All three Neo boards integrate a graphics processor with 2D/3D graphics acceleration and include a micro HDMI port and LVDS interface.

The UDOO Neo Basic includes 512 MBytes of DDR3 RAM and features 10/100 Ethernet. The Neo Extended offers 1GByte of DDR3 RAM, as well as 802.11 b/g/n Wi-Fi and Bluetooth 4.0 Low Energy connectivity. The Neo Full includes the same features as the Extended and adds 10/100 Ethernet, as well as nine-axis motion sensors (accelerometer, gyroscope, magnetometer) for Internet of Things (IoT) applications.

The UDOO Neo boards support many development environments (including Arduino, Python, and PHP), plus support for Android Lollipop and UDOObuntu2 — the official UDOO distribution of the Lubuntu Linux operating system.

To learn more about the UDOO Neo boards, visit http://www.mouser.com/new/udoo/udoo-neo/. For more information on the full lineup of UDOO single-board computers available from Mouser Electronics, visit http://www.mouser.com/new/udoo/udoo-dual-quad-neo/


With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About UDOO
UDOO is a community of passionate makers, creative students and designers with expertise in interaction design, embedded electronics, sensor networks and cognitive science. UDOO is also a family of products that share a playful approach to physical computing with easy, open-source tools and cutting-edge enabling technologies.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President, Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room